VirtualSerial Device Example: USB-UART Bridge Task for LPC11U14?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VirtualSerial Device Example: USB-UART Bridge Task for LPC11U14?

1,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Fulbag on Sat Oct 13 08:17:02 MST 2012
Hello,
I was going to test the VirtualSerial Device Example (nxpUSBlib v0.97) with my LPC11U14 LPCXpresso, but I just noticed that in the VirtualSerial.c file it is reported the following statement:
---------------------------
[...]

/** Select example task, currently lpc11Uxx and lpc17xx don't support for bridging task
* Only LPC18xx has this feature */
#define CDC_TASK_SELECTECHO_CHARACTER_TASK

[...]
---------------------------

Do you confirm that the USB-UART Bridge Task is not available for LPC11U14 yet?

Thank you.

Best regards,
Fulvio
标签 (1)
0 项奖励
回复
0 回复数