Virtual COM using LPCOpen example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Virtual COM using LPCOpen example

1,465 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Idanba on Sun Apr 19 07:03:40 MST 2015
Hi,

I'm running the usbd_rom_cdc_vcom example and wondering whether a call-back for closing the virtual COM port is also available and not only upon opening it ( cdc_param.SetLineCode = VCOM_SetLineCode )

Thanks!
Idan
Labels (1)
0 Kudos
Reply
2 Replies

1,431 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Idanba on Sun Apr 19 22:00:01 MST 2015
sorry :)

It's LPCOpen 2.12 and I'm running it on a LPC4357 MCU using keil evaluation board (MCB4300).  The IDE is Keil's MDK4.
0 Kudos
Reply

1,431 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Apr 19 07:20:22 MST 2015

Quote: Idanba
I'm running the usbd_rom_cdc_vcom example...



Any hints about the mcu?
0 Kudos
Reply