VREFP shut down external reference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VREFP shut down external reference

1,055 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by uknoblic on Tue Mar 11 07:59:45 MST 2014
Hi,

we decided to use a LM4040 external voltage reference (2.5 V) connected to the VREFP pin. Depending on the shunt resistor this voltage reference draws something above 60 µA which is not acceptable for our battery driven application. Our idea is to provide the LM4040 supply voltage from any LPC1768 pin and shut down the reference when the ADC is not needed. Is there something to consider using this approach?

Regards

Ulf
Labels (1)
0 Kudos
Reply
1 Reply

1,037 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Apr 04 16:42:44 MST 2014
Hi, Ulf,

We will check with the designer and see if the 60uA is reasonable for this part. This is not specified in the Datasheet and IP specification.

Thanks,
0 Kudos
Reply