VCOM driver for LPC1549

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VCOM driver for LPC1549

3,125 Views
emitterLCR
Contributor I

I downloaded the LPCOpen to use the smple code of VCOM function for LPC1549.

LPCOpen Software for LPC15XX | NXP Semiconductors

In the readme.txt, inf file is needed when I connect to the Windows host.

But I couldn't find the .inf file in LPCOpen zip file.

 

*Special connection requirements:
--------------------------------
Connect the USB cable between micro connector on board and to a host.
When connected to Windows host use the .inf included in the project
directory to install the driver. For OSx (Mac) host, no drivers are needed.

-----------------------------------------------------------------------------------------------------------

Where is the .inf file ?  or Where is the download link in the HP?

I'd like the help and information..

 

0 Kudos
Reply
2 Replies

3,112 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

i suppose that the *.inf file for USB is defined/saved/run in PC side instead of MCU side, generally, you can use default *.inf file.

BR

XiangJun Rong

0 Kudos
Reply

3,061 Views
emitterLCR
Contributor I

Sorry for replying late.

I could use the standard driver on Windows.

The driver was installed automatically.

Thank you !

0 Kudos
Reply