Using the MDK project in the SDK package, but the program download does not enter Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the MDK project in the SDK package, but the program download does not enter Flash

2,086件の閲覧回数
nuaamessi
Contributor I

The model of the development board is LPCXpresso54S018M, as shown in Figure 1, which is the corresponding package I installed. Figure 2 shows the configuration of flash, as shown in Figure 3, using microusb to connect to the Debug Link, and Figure 4 shows the DAP emulator. Now the code can be debugged normally, but as shown in Figure 5, error will be reported when downloading. I don't know how to solve this problem, I hope my friends can help me, thank you very much!

1685538966116.png1685539275408.png02219a481d8763c2fa1876c3b59945f.jpg1685539656330.png1685539728162.png

ラベル(1)
0 件の賞賛
返信
1 返信

2,061件の閲覧回数
CarlosGarabito
NXP TechSupport
NXP TechSupport

As far as I can see, you are using only the debug, you need to power the board with the power cable, I recommend you to read the start quick guide of this board. https://www.nxp.com/document/guide/get-started-with-the-lpc54s018m-evk:GS-LPC54S018M-EVK

0 件の賞賛
返信