Using the LPC54608 for senior design project: Virtual Drum

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the LPC54608 for senior design project: Virtual Drum

1,112 Views
andrewliu
Contributor I

Our senior design project was to create a virtual drum.

Digital Drum - Dem boys - YouTube 
Here's a short video demonstration of the final design in action.

The input is a cheap piezoelectric microphone, which transmits the signals to the LPCXpresso 54608 board. The board is used to read the data (mainly the intensity of each hit) and output a snare drum sound corresponding the intensity of the hit.

I've attached the report for our final design, with an explanation of how the code works.

The code can be found here: Demboys/README.md at master · hwebin/Demboys · GitHub

0 Kudos
Reply
1 Reply

1,026 Views
soledad
NXP Employee
NXP Employee

Hi Andrew,

Thank you for your input.

Regards

Sol

0 Kudos
Reply