Using mxli with LPC1837

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using mxli with LPC1837

2,580件の閲覧回数
johnisaac
Contributor I

Trying to see if I can program a LPC1837 with mxli.   

# ./mxli -n -d /dev/ttyS0 -b 115200 -c 12000000 -g
?\x0D\x0A\x0DLINE BREAK:\r
ERROR: pattern "Synchronized" not found, Fifo was ""
ERROR: No or invalid response

Any idea what I might be doing wrong?  

#mxli

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,386件の閲覧回数
johnisaac
Contributor I

I got it working.  The problem was that I wasn't holding the ISP pin long enough on the reset.    

0 件の賞賛
返信

2,386件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi John,

It is good to hear you got it working.

Best Regards!
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

2,386件の閲覧回数
johnisaac
Contributor I

I have some additional information that may be useful.  

For some reason I am able to access the UART command handle using a standard terminal and commands (See Table 27 Section 5.7 LPC18xx ARM Cortex-M3 microcontroller User's Guide) so I know I'm talking the the ISP command handler.     For some reason the "?" synchronization handshake is not working and hence this is why mxli doesn't work.   Interestingly enough I'm having the same issue with lpc1isp.    There is a discussion in 5.4.4.1 that discussed this synchronization step but it appears I don't need this to access the ISP command handler.   

0 件の賞賛
返信