Using Yaffs file sytem ....project takes more than two minute to initilize it..??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Yaffs file sytem ....project takes more than two minute to initilize it..??

1,029件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by studyembedded on Thu Nov 14 00:56:53 MST 2013
Hi Friends,
I am working on a project using LPC1788. On my board we have a NAND flash K9F1G08X0C and trying to add a file system.
I am using a Yaffs file system. Everything is ok I am able to mount, write and read and display the data as well. The only problem is it takes more than two min to display it on TFT. I mean to say it takes almost more than two min to initialize the project.

I am unable to understand how to speed it, according to Yaffs document it should start within few seconds, with that my project boots properly.

Please help me!!
ラベル(1)
0 件の賞賛
返信
0 返答(返信)