Using USB Memory Sticks with LPC32XX Device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using USB Memory Sticks with LPC32XX Device

1,094 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rcsison on Fri Jun 01 08:33:41 MST 2012
We are using a Phytec development board based on the LPC3250. We are using the Adeneo BSP for this, which as the default setting as Active Sync, the target board directory contents being visible to a PC connected to the Phytec board through the Active Sync connection.

If we want to be able to use USB memory sticks / flash drives instead, what does this entail? New drivers? Registry updates? For WinCE users, the proper selections in the Catalog Items? For USB Function Clients (Mass Storage)and USB Host?

The upshot: is it possible to set up an LPC3250-based device so that it can recognize USB memory sticks and allow the application to read from them and write to them?

Thanks for any advice out there...
Labels (1)
0 Kudos
Reply
0 Replies