Using UARt1 with full modem RS232 interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using UARt1 with full modem RS232 interface

897 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wafa on Thu Mar 28 01:18:59 MST 2013
I have a Embedded Artists’ LPC1788 development board and I was successful to download the Example USB_VirtualCom. This example does not go with the RS232 interface. How do I modify the program or is there another example that does use UART1 to connect with full modem RS232 interface.
标签 (1)
0 项奖励
回复
0 回复数