Using UARt1 with full modem RS232 interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using UARt1 with full modem RS232 interface

895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wafa on Thu Mar 28 01:18:59 MST 2013
I have a Embedded Artists’ LPC1788 development board and I was successful to download the Example USB_VirtualCom. This example does not go with the RS232 interface. How do I modify the program or is there another example that does use UART1 to connect with full modem RS232 interface.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)