Using SGPIO14/15 to trigger 2 DMA transfers??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using SGPIO14/15 to trigger 2 DMA transfers??

1,144件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rnunes on Tue Apr 07 16:04:50 MST 2015
I'm using LPC4337 and I was trying to find a way to have SGPIO14 or 15 triggering 2 distinct DMA transfers at the exact same time (otherwise it's useless). As far as the User Manual goes I don't see anything saying that it can or cannot, can you help me with this?

Thanks
ラベル(1)
0 件の賞賛
返信
1 返信

1,133件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Thu Apr 09 17:43:54 MST 2015
It may work if we define SGPIO14 and SGPIO15 as parallel input. They should synchronize the trigger.
0 件の賞賛
返信