Using RI timer LPC1317

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using RI timer LPC1317

1,980件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aamir ali on Wed Jul 31 05:17:37 MST 2013
UM10524 says that "Power to the register interface (RI timer clock): In the SYSAHBCLKCTRL register, set
bit 25 in Table 19."

But bit25 in SYSAHBCLKCTRL  is reserved. So how to enable clock to RI timer.

Is there example code available. I didn't find example of RIT in keil example codes
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,865件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aamir ali on Wed Jul 31 21:51:08 MST 2013
Hi,
I had older version of UM which had this error. In newer version of UM this has been removed.

Thanks.
0 件の賞賛
返信

1,865件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tha on Wed Jul 31 10:53:15 MST 2013
Can you double check on that?  I did a search for the phrase "Power to the register interface" and the only area that show up is Chapter 15.2 on page 300.  In that area, it says bit 15, not bit 25.
0 件の賞賛
返信