Using ISP "G 0 T" command on LPC1549

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using ISP "G 0 T" command on LPC1549

1,203 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by randyd on Thu Nov 27 14:32:30 MST 2014
Hello,

I've written a factory programer in Python to serial ISP flash our LPC1549 and LPC1115.
After flashing, the LPC1115 user code can be started without a power cycle or reset symply by issuing the "G 0 T" ISP command,
however this does not work with the LPC1549 and it appears to hang, I've also tried "G 0 A".
I'm unable to find what the difference is after reading the user manuals, if someone could point me to another appnote or give advice I'd appreciate it.
Thanks,
Randall.
标签 (1)
0 项奖励
回复
0 回复数