Update FreeRTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update FreeRTOS

1,234 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GPh on Tue Apr 28 00:53:00 MST 2015
Hi,

We are using LPCOpen with FreeRTOS.
But the version provide in LPCOpen is 7.5.3

Can we update with 8.2 ?
Is there good reason for use the old version ?

Thanks a lot.
Philippe.
Labels (1)
0 Kudos
Reply
1 Reply

1,226 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by www.FreeRTOS.org on Wed Apr 29 02:17:36 MST 2015
The only thing that could cause an issue would be if LPCOpen was giving a mutex from an interrupt where things have changed - other than that you should find you can just drop the latest FreeRTOS files into your project, overwriting the previous file (back the previous files up first, naturally!).
0 Kudos
Reply