Unused Pins of LPC4322 Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unused Pins of LPC4322 Microcontroller

Jump to solution
1,163 Views
SrinathVelavan
Contributor III

How do we configure the unused pins on an LPC4322 Microcontroller? At present, I have left them unconnected with no-connect on schematic for my board.

Labels (1)
0 Kudos
Reply
1 Solution
1,138 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

All I/Os default to input with pullup after reset. So it has internal pullup.

For non-opendrain GPIO, left unconnected if driven LOW and configured as GPIO output with pull-up or pull-down disabled by software. Or just default setting (input with pullup) is ok

For opendrain GPIO, left unconnected if driven LOW and configured as GPIO output by software.

Please follow below to configure the unused pins.

ZhangJennie_0-1684669075172.png

Hope this helps,

Jun Zhang

 

View solution in original post

2 Replies
1,139 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

All I/Os default to input with pullup after reset. So it has internal pullup.

For non-opendrain GPIO, left unconnected if driven LOW and configured as GPIO output with pull-up or pull-down disabled by software. Or just default setting (input with pullup) is ok

For opendrain GPIO, left unconnected if driven LOW and configured as GPIO output by software.

Please follow below to configure the unused pins.

ZhangJennie_0-1684669075172.png

Hope this helps,

Jun Zhang

 

1,111 Views
SrinathVelavan
Contributor III

Thank you for your answer.

0 Kudos
Reply