Unstable RAM access after changing speed to 204MHz

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unstable RAM access after changing speed to 204MHz

1,059 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Jon Reece on Wed Mar 27 02:36:30 MST 2013
Hi,

I am using an EA OEM board for an application and I am trying to increase the speed of the processor to reduce the processing time. I have successfully changed the clock speed in steps following the BlickFast example. When I query the clock speed I now get 204000000 as expected. However, when I try and access the SDRAM the processor will disconnect from the debugger and I cannot stop/reprogram it.

Do you have an example of setting up the SDRAM peripheral to work at 102MHz with a core clock of 204MHz? The ISSI RAM chip that we are using, IS42S32800D-6BLI, should support bus speeds of upto 166MHz so I don't believe that 102MHz should be a problem. I am using the NS2CLK function to get the register timing values which implies that I should be able to change the clock speed and the ram *should* (as I understand it) work.

If you need any more information please let me know,

Thanks
Jon
标签 (1)
0 项奖励
回复
3 回复数

1,008 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hlsa on Fri Apr 19 02:36:55 MST 2013

This is a known problem of the EA-Board. I have already addressed this issue to EA in february and they confirmed the problem. As far as I know, there is still no solution (what a shame for EA). SDRAM works here only up to 144 MHz.


In the meantime I bought an evaluation board from Keil (MCB4357) and I do have my own hardware. On both of the SDRAM works fine. 


 


Best regards,


Holger 

0 项奖励
回复

1,008 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larsjep on Wed Apr 03 02:10:38 MST 2013
Hi,

Please notice that LPC43xx has a problem with the EMC clock divider.
When the clock divider is enabled the duty cycle of the EMC clock is not 50%
This can result in problems with the required setup times of the address signals.

Regards
  Lars
0 项奖励
回复

1,008 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by suckfish on Mon Apr 01 15:59:30 MST 2013
Everything locking up when you access SDRAM could well be a clocking problem.

Check that you have all 4 EMC clock outs going to the pins, and that you have the *input* buffers enabled on those pins also.

[It's counter-intuitive that you need all 4, and that you need them as inputs also, but yes you do.  Presumably the EMC is using the inputs as feedback to adjust timing.]
0 项奖励
回复