Unresponsive LPC5504

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unresponsive LPC5504

1,158 次查看
lumine01
Contributor I

LPC5504 is giving me headaches. My code is working fine with MCUXpresso IDE and runs flawlessly. However, the moment I power cycle the board, the firmware disappears! The chip becomes completely unresponsive, and I have to re-flash it. I have tried everything, including different LPC5504 boards, various power supplies, and double-checking the boot pins. But nothing seems to work. My Stonegrill restaurant is lacking behind because of this. Is there someone else who faces similar issues?

0 项奖励
回复
2 回复数

1,128 次查看
ErichStyger
Specialist I

Just asking the obvious: are you sure you have programmed the FLASH memory with your application, and that you are *not* running a RAM target?

0 项奖励
回复

1,131 次查看
lumine01
Contributor I

I would really appreciate if someone could help me find a solution since my Stonegril restaurant is suffering because of this.

0 项奖励
回复