Unresponsive LPC5504

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unresponsive LPC5504

1,133件の閲覧回数
lumine01
Contributor I

LPC5504 is giving me headaches. My code is working fine with MCUXpresso IDE and runs flawlessly. However, the moment I power cycle the board, the firmware disappears! The chip becomes completely unresponsive, and I have to re-flash it. I have tried everything, including different LPC5504 boards, various power supplies, and double-checking the boot pins. But nothing seems to work. My Stonegrill restaurant is lacking behind because of this. Is there someone else who faces similar issues?

0 件の賞賛
返信
2 返答(返信)

1,103件の閲覧回数
ErichStyger
Specialist I

Just asking the obvious: are you sure you have programmed the FLASH memory with your application, and that you are *not* running a RAM target?

0 件の賞賛
返信

1,106件の閲覧回数
lumine01
Contributor I

I would really appreciate if someone could help me find a solution since my Stonegril restaurant is suffering because of this.

0 件の賞賛
返信