Unable to read GPIO pins.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to read GPIO pins.

1,380件の閲覧回数
vxs187
Contributor III

I am not understanding how to read GPIO pins using the LPC 4370, I am unable to get the right reading. I am trying to give a DC supply but am not able to get any proper output, it always gives me 0, meaning the input is always low, even when I am giving a DC of 3.3V. Do I have to supply a greater voltage? I am totally left clueless. I am using GPIO1_0.

0 件の賞賛
返信
1 返信

1,271件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

I suggest to use the LPCOpen Blinky example, the blinky example flashes an LED in a periodic rate. 

You can download LPCOpem from the following link:

LPCOpen Software for LPC43XX|NXP 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信