Unable to program lpc1788 with Flash magic in ISP mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to program lpc1788 with Flash magic in ISP mode

3,284 Views
atihaj
Contributor I

Hi  MCUXpresso Software and ToolsLPC

I developed a firmware in lpcxpresso for LPC1788(generated hex file).

Then I want to program it with Flash magic. 

But unable to program during programming, it erase the blocks and while programming initiate it wait for a while and prompt "Programming Failed [Program failed to send data to the device". 

communication through Flash magic terminal is done and it seems controller response to ISP commands.

Please suggest if any solution have.

Regards

Ati

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

2,316 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link:

[LPC1788] programming - failed to send data to the device 

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply