Unable to program lpc1788 with Flash magic in ISP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to program lpc1788 with Flash magic in ISP mode

3,204件の閲覧回数
atihaj
Contributor I

Hi  MCUXpresso Software and ToolsLPC

I developed a firmware in lpcxpresso for LPC1788(generated hex file).

Then I want to program it with Flash magic. 

But unable to program during programming, it erase the blocks and while programming initiate it wait for a while and prompt "Programming Failed [Program failed to send data to the device". 

communication through Flash magic terminal is done and it seems controller response to ISP commands.

Please suggest if any solution have.

Regards

Ati

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

2,236件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link:

[LPC1788] programming - failed to send data to the device 

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信