Unable to program LPC1547 using Flash Magic

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to program LPC1547 using Flash Magic

1,560 次查看
gouthamuttarkar
Contributor I

Crystal 16MHz

Hex file 8KB

I am using USB UART Bridge to program LPC1547 

I have successfully programmed it two days ago and now it's causing problems.

The microcontroller is not responding to "?" For autobaud 

标记 (2)
0 项奖励
回复
1 回复

1,442 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please try with an ISP reset,  check the following thread,

https://community.nxp.com/thread/389040 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复