Unable to program LPC1347 using JTAG pins.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to program LPC1347 using JTAG pins.

3,659件の閲覧回数
shreelaxminair
Contributor I

Hi all,

I am using LPC1347. In this controller TMS and SWDIO are not multiplexed.

So I have used Ulink Pro to program the controller via JTAG. However the device does not get detected via JTAG. Programming via SW is possible though. Can any one help and explain why programming via JTAG is not happening?

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

3,452件の閲覧回数
thefallguy
Contributor IV
0 件の賞賛
返信

3,449件の閲覧回数
shreelaxminair
Contributor I

Ok

0 件の賞賛
返信

3,449件の閲覧回数
rolfmeeser
NXP Employee
NXP Employee

The JTAG port provides access to boundary scan only.

CPU debugging and flash programming can be done solely through the SWD port.

This is not an SWJ-DP.

0 件の賞賛
返信

3,449件の閲覧回数
shreelaxminair
Contributor I

Thanks for the reply.

By the way how does debugging & boundary scan differ from each other?

0 件の賞賛
返信