Un-bonded Pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Un-bonded Pins

2,410件の閲覧回数
bob_walker
Contributor III

LPC 8xx devices...

Does anyone know if it is possible to use unbonded pins for routing via the SWM block and various block inputs WITHOUT using existing bonded pins? Are these unbonded I/Os still available on packages with low pin count?

0 件の賞賛
返信
2 返答(返信)

2,336件の閲覧回数
bob_walker
Contributor III

Kerry,

An un-bonded pin is the example you just gave. PIO0_20 does not exist on the package (un-bonded). However, it does exist on the chip. This is the answer I was looking for. Thanks.

0 件の賞賛
返信

2,336件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Bob_walker,

   Actually, SWM is defined the according internal block interface to the detail chip pin, PIO0_0 to PIO0_28.

  What do you mean:unbonded I/O?

  Do you mean? Take an example:

pastedImage_1.png

    This pin don't have PIO0_20, but if you use SWM connect the internal block, various block, no external pin, but the internal different block will be connected.

    This picture may help you to understand it.

pastedImage_2.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信