Uart not displaying data in terminal window

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uart not displaying data in terminal window

1,313 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marvic on Wed Aug 06 06:49:43 MST 2014
Hi,

I am using LPC mx-1114/301 board. Small piece of code written to send and receive the data to and from Hyper terminal.
Output, not showing typed data on terminal window. Any problem in source code? Can be appreciated to sort me out this. Here the code,


#include"lpc11xx_syscon.h"
#include"lpc11xx_gpio.h"
#include "lpc11xx_uart.h"
#include "LPC11xx.h"

#define SystemCoreClock 12000000UL
#define RDR 0x01
#define THRE 0x20


int main(void)
{
   unsigned char data;
   uint32_t  baudrate = (uint32_t)115200 ;
   uint32_t  DL;

   LPC_IOCON->PIO1_6 = 0x01;
   LPC_IOCON->PIO1_7 = 0x01;

   LPC_SYSCON->SYSAHBCLKCTRL |= (1<<12);
   LPC_SYSCON->UARTCLKDIV = 0x01;        //UART clock
   DL = (SystemCoreClock * LPC_SYSCON->SYSAHBCLKDIV) / (16 * baudrate * LPC_SYSCON->UARTCLKDIV);
   LPC_UART->LCR = 0x83; //0x10000011; 
   LPC_UART->DLM = 0x01; //DL / 256;   
   LPC_UART->DLL = 0x86; // DL % 256;  
   LPC_UART->LCR = 0x03; //0x00000011;
   LPC_UART->FCR = 0x07; //0x00000111; 

   while(1){

   while (!(LPC_UART->LSR & RDR));
        data = LPC_UART->RBR;

      while (!(LPC_UART->LSR & THRE));
       LPC_UART->THR = data;
    }
}

Thanks,
Labels (1)
0 Kudos
Reply
1 Reply

1,277 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Thu Aug 07 17:55:52 MST 2014
Hi,

Is there a specific reason for why you are writing your own code for UART? In case you did not know, we have a software platform called LPCOpen and there will be various drivers, including UART. You can download the platform here:
http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc11xx-packages-0

It does not seem like your board is supported, but the base UART initialization should be the same across all LPC11xx. As for debugging your current program, do you have access to an oscilloscope or logic analyzer? I would try to see if you initialized the UART correctly. Also make sure your initializing the same UART pins as the one that is connected to your computer!
0 Kudos
Reply