Uart Debugging messages in lpc4330 xplorer board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Uart Debugging messages in lpc4330 xplorer board

580件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by praveen.9123 on Mon Feb 24 23:26:39 MST 2014
Hi,
     Can you please help in debugging print messages for ngx lpc4330 xplorer board.
I am using TTL to RS232 board and connected to Serial cable. And Configured the pins as follows.
I have flashed uart example which is given by ngx.
The following link contains examples.


Serial cable pins as follows in lpc4330 xplorer board
====================
J10.16 Tx board -> TTL to RS232 Rx.
J10.26 Rx  board -> TTL to RS232 Tx.
J10.2 Vcc  board -> TTL to RS232 Vcc
J8.1 Gnd  board -> TTL to RS232 GNd.

Where can i get the Debug messages in PC and how can i see that debug messages.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)