USBD ROM stack: CDC class NCM support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBD ROM stack: CDC class NCM support

ソリューションへジャンプ
2,784件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ZZZMQP on Sat Mar 19 17:19:22 MST 2016
Hello,

I'm looking for NCM support (Ethernet-over-USB) for the CDC class. Does anyone have any information if this is supported in the USBD ROM stack directly, or where to get it?

Cheers,
  Dusty.
ラベル(1)
  • USB

0 件の賞賛
返信
1 解決策
2,567件の閲覧回数
ckphua
NXP Employee
NXP Employee

This is not supported in USB Device ROM stack.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,568件の閲覧回数
ckphua
NXP Employee
NXP Employee

This is not supported in USB Device ROM stack.

0 件の賞賛
返信
2,567件の閲覧回数
gregdunn
Contributor I

Any luck with adding NCM support?

Thanks,

Greg

0 件の賞賛
返信
2,567件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信