USB1 boot is not function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB1 boot is not function

1,309 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nagar.sumit on Tue Feb 09 02:39:08 MST 2016
Hello All,

Can anyone tell me the technical reason behind not working condition of USB1 boot?

I  was reading Errata for LPC4350 and i found out that USB1 boot is not functional and it is telling to USB0 instead of USB1.

I am very curious to understand limitation of booting with USB1.

Looking forward to reply

Thanks and Regards,
Sumit Nagar
标签 (1)
0 项奖励
回复
2 回复数

1,299 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nagar.sumit on Tue Feb 09 20:20:35 MST 2016
Hello,

Thanks for your reply, it is understandable that there is a bug in BOOT rom code, but what is it? Why is it only on USB1 and not on USB0?

Is there any any future revision of MCU plan for resolving this BUG of Boot on USB1?

Thanks and Regards,
Sumit Nagar
0 项奖励
回复

1,299 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Tue Feb 09 06:14:08 MST 2016
Given that it is the errata, it is probably just a bug in the boot rom code. Afaik, the usb1 port works apart from this boot limitation.
0 项奖励
回复