USB0_VBUS active components

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB0_VBUS active components

1,856 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Wed Mar 18 13:38:38 MST 2015
Hi,

Having trouble reading section 22.5.1 in the LPC18xx users manual. 

I am using USB0 for a device connection with a type A connector.  My unit can be USB powered.
The paragraph says that I may need to add active components to disconnect the link when VDDIO
is not present.  Not sure what that means for my application.

My VDDIO comes from an LDO hung on USB_VBUS so it may lag it a little ( probably only 10s of nanoseconds ).  However
VDDIO is always present once the USB power is available.

Do I need to disconnect USB0_VBUS from the USB supplied 5V power durring the power up sequence?

Thanks
标签 (1)
0 项奖励
回复
2 回复数

1,834 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Thu Mar 19 05:23:35 MST 2015
Thanks!
0 项奖励
回复

1,834 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Wed Mar 18 16:30:16 MST 2015
Consider the time is very short when VDDIO lags behind VBUS, this is probably fine.
regards,
0 项奖励
回复