USB vcom port conflict with timer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB vcom port conflict with timer

1,842件の閲覧回数
thoret
Contributor II

Hi,

I use the LPC1769. I built a project ro control 3 servo motors.

I communicate over a usb virtual com port with my computer.

If I start my programm and setup the usb first and after the pwm signal, the usb port is disconnected.

If I change it and setup the pwm first , it works.

But now I have to setup a timer. I setup the timer before the usb setup and after but the usb vcom port is not connectet to the computer.

I try to use the timer o and timer 1, but it dosn't help.

I use the cmsisv2p00 libary.

For my usb vcom port I implemented the RDB1768cmsis2_usb_serial and RDB1768cmsis2_usbstack example.

ラベル(3)
0 件の賞賛
返信
1 返信

1,396件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Thore,

The use of LPCOpen is now recommend for most LPC MCUs, rather than the 'old-style' CMSIS-CORE library projects and examples. I would recommend you to download the LPC17xx LPCOpen package from this link:

LPCOpen Software for LPC17XX|NXP 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信