USB on LPC54016JET100 with Vdd=1.8V

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB on LPC54016JET100 with Vdd=1.8V

3,510 次查看
andrewsglenn
Contributor III

We'd like to use the LPC54S016JET100 with Vdd=1.8V to interface with all our 1.8V peripherals.

Looking at the LPC540xx data sheet Table 12, minimum Vdd for USB Full Speed is 3.0V, but for High Speed is 1.71V, implying we should use USB1 for our interface.

My question is what happens if a Full-Speed device is connected to the High-Speed interface? Does it fail to enumerate as it needs a higher voltage? 

What are the limitations of trying to use USB1 at 1.8V?

0 项奖励
回复
9 回复数

3,485 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @andrewsglenn 

1> "My question is what happens if a Full-Speed device is connected to the High-Speed interface? Does it fail to enumerate as it needs a higher voltage? "

->> My understanding is that, for the working voltage of USB0( Full- speed) is 3.0 -3.6v.

The working voltage of usb1 is 1.71 - 3.6V.

2> "What are the limitations of trying to use USB1 at 1.8V?"

->> I.8v is the normal voltage limits.

 

BR

Alice

0 项奖励
回复

3,479 次查看
andrewsglenn
Contributor III

So if you're using USB1 and it is connected in Full Speed mode rather than High Speed (due to limitations of the device connected) It will still work at Full Speed?

0 项奖励
回复

3,461 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @andrewsglenn 

Yes, it will work as full speed.

And for Full Speed operation, VDD must be min of 3V. 

 

BR

Alice

0 项奖励
回复

3,416 次查看
andrewsglenn
Contributor III

Here's our setup:

VDD is 1.8V

USB1_AVDDC3V3 is 3.3V

USB1_AVDDTX3V3 is 3.3V

 

From what you are saying, USB1 will work as a High-Speed device, but will fail as a Full-Speed device because VDD is not 3V or higher?

Is this correct?

0 项奖励
回复

3,391 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @andrewsglenn 

If USB1 works as Full- speed device, 

VDD is 1.8V

USB1_AVDDC3V3 is 3.3V

USB1_AVDDTX3V3 is 3.3V

 

Yes, USB1, will work.

 

BR

Alice

0 项奖励
回复

3,392 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @andrewsglenn 

There is a little bit confusing and sorry about this, I will confirm with our internal.

 

BR

Alice

0 项奖励
回复

3,292 次查看
andrewsglenn
Contributor III

Any luck finding a definitive answer?

0 项奖励
回复

3,242 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @andrewsglenn 

Please see my reply last  time:

Alice_Yang_0-1708306620170.pngAlice_Yang_0-1708306620170.png

 

BR

Alice

0 项奖励
回复

3,381 次查看
andrewsglenn
Contributor III

Thank you.

0 项奖励
回复