USB module communication on HITEX LPC4350 evaluation board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB module communication on HITEX LPC4350 evaluation board

1,033件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sooraj on Tue Jun 14 20:54:23 MST 2016
Hello,

In the Hitex lpc4350 evaluation board, I have noticed that USB 0 section of LPC controller has signals like USB0_VBUS, USB0_RREF, USB0_VDDA_3V3_DRIVER, USB0_VDDA3V3, USB0_VSSA_TERM, USB0_VSSA_REF , while USB1 doesnt have these extra signals.

What will be the effect if  these signals are absent for USB0 i.e. I dont connect these pins at all, leave them open. How it will affect my circuit. I am studying the circuitry on the board, so I would like to know what happens when some signals are missing.

Please help me with this.


Thanks and Regards,

Sooraj.
ラベル(1)
0 件の賞賛
返信
1 返信

982件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信