USB mass storage sdmmc example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB mass storage sdmmc example

950 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by joepbrown on Wed Feb 20 18:19:56 MST 2013
I've been working for a few days to get the LPCOpen_platform USB mass storage(sd/mmc support) example running in my code-red compiler but have had many issues. I'm wondering if anyone knows of a good library that supports USB mass storage on an sd/mmc card that they've got up and running with LPCxpresso/code-red?

Also, does anyone know where I can check the development status of LPCOpen? I see that all LPCxpresso/code-red examples were removed in 1.00 (this link: http://www.lpcware.com/content/page/lpcopen-releases-and-versioning-information), and it says they'll be back in V1.1, but I have no idea who is working on that project and when they expect to release future versions.
标签 (1)
0 项奖励
回复
1 回复

902 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Thu Feb 21 11:56:00 MST 2013
>Xpresso support returning in v1.01
The LPCOpen pages were just updated with additional information.
http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-upcoming-re...

(Improved) Xpresso support should be restored in v1.01 for the 18xx/43xx. v1.01 should be released next week.
0 项奖励
回复