USB mass storage device sample?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB mass storage device sample?

1,985 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tamirmichael on Fri Apr 13 07:56:00 MST 2012
Hello,

Maybe I missed something huge, but there seem to be no sample file attached to this page:

http://www.lpcware.com/content/page/mass-storage-device-example

I would like to see the an implementation of a USB mass storage device for a LPC1788.

Thanks in advance!
Labels (1)
0 Kudos
Reply
3 Replies

1,760 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tamirmichael on Sat Apr 14 04:06:09 MST 2012
Thank you very much.
0 Kudos
Reply

1,760 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpUSBlib team on Fri Apr 13 17:07:54 MST 2012
You will see an implementation of a USB mass storage device by downloading the package from here : http://www.lpcware.com/content/nxpfile/nxpusblib-v093
To get start you should visit the main page (http://www.lpcware.com/content/project/nxpusblib) and follow the steps:

Get it
Build it
Use it

0 Kudos
Reply

1,760 Views
gchristopher
Contributor I

These links seem to be dead now. Is the nxpUSBlib project abandoned? (Googling it and searching community.nxp.com didn't help.)

Is there an nxp library that supercedes it? This was the only mass storage device example I could find.

0 Kudos
Reply