USB mass astorage device does not work on windows XP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB mass astorage device does not work on windows XP

1,235件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tamirmichael on Tue Apr 17 00:39:32 MST 2012
Hello,

I'm trying the USB mass storage device sample available in the CMSIS driver library:

http://sw.lpcware.com/?p=lpc177x_8x.git&a=summary

on a LPC1788. It does seem to work correctly on Windows 7, but when connected to a Windows XP machine an error is reported when the drive is accessed, and its label is not displayed correctly. I tried to replace the descriptors with a set that does work with Windows XP (LPC2478 device) but that does not help.
I did not monitor the USB bus yet.

Thanks in advance
ラベル(1)
0 件の賞賛
返信
1 返信

1,225件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tamirmichael on Tue Apr 17 00:57:41 MST 2012
Solved using http://www.lpcware.com/content/nxpfile/nxpusblib-v094
0 件の賞賛
返信