USB hub support for lpc4337

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB hub support for lpc4337

2,174 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhall0819 on Mon Feb 03 14:53:37 MST 2014
Hi,
I am using and lpc4337 along with LPCopen V 2.04. The project needs to connect my 4337 host to 4 USB devices through a hub. We have a Cypress hub chip connected to USB0.

I have tried the LPCopen example for host keyboard on USB1. Would like to extend this through a hub. Are there LPCopen updates, app notes, or any documentation, or 3rd party packages that would shed some light on firmware that would support connections through a hub.

Thanks  
Labels (1)
0 Kudos
Reply
2 Replies

1,897 Views
k2
Contributor III

John,

I'm in need of HUB support for the LPC4337 also.

Did you ever find anything ?

I got the hub code working in my LPC54608 design,

but back porting to the LPC4337 looks ugly.

Hoping you found something ....

Kevin

0 Kudos
Reply

1,898 Views
k2
Contributor III

I ended up writing a HUB app for the LPC4337.

wasn't as bad as i thought.

It has TT support as well. I'm using a 4 port SMSC hub.

Kevin

0 Kudos
Reply