USB host (for MSD) example and test problem at USB1 interface in LPC54618.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB host (for MSD) example and test problem at USB1 interface in LPC54618.

Jump to solution
3,264 Views
toipaz
Contributor III


1. Environment:

SDK v2.9.0
CPU: LPC54618
example Code: host_msd_fatfs_freertos

2. Goal: USB 2.0 Host MSD @ USB1 interface

3. Problem

The example code only supports OHCI.

Referring to Datasheet, USB1 is EHCI compliant.
Using EHCI in the example, it is not built with a compile error saying that there is no ehci driver source.

4. Questions

4.1. When using usb1 interface, does it work with ohci?

4.2. Can I specify that the example source uses usb1 interface?

attachement: test project code.

 

0 Kudos
Reply
1 Solution
3,243 Views
toipaz
Contributor III

The USB hw block did not work properly because the GND wiring of the USB circuit was connected incorrectly.
Corrected the GND wiring and it worked normally.

View solution in original post

0 Kudos
Reply
2 Replies
3,257 Views
toipaz
Contributor III

As I looked at the datasheet and manuals, it says that it uses USB_HOST_CONFIG_IP3516HS.

So

in usb_host_config.h, we test it by changing it as follows.:

#define USB_HOST_CONFIG_OHCI (0U)
#define USB_HOST_CONFIG_IP3516HS (1U)

After that, it'll be waiting forever at the while() statement in usb_host_ip3156hs.c as below.:

static usb_status_t USB_HostIp3516HsControllerReset(usb_host_ip3516hs_state_struct_t *usbHostState)
{
    usbHostState->usbRegBase->USBCMD = USB_HOST_IP3516HS_USBCMD_HCRESET_MASK;
    while (0U != (usbHostState->usbRegBase->USBCMD & USB_HOST_IP3516HS_USBCMD_HCRESET_MASK))
    {
        __NOP();
    }
    return kStatus_USB_Success;
}

The USB1 RESET command is not completed, where should I start to find bug?

0 Kudos
Reply
3,243 Views
toipaz
Contributor III

The USB hw block did not work properly because the GND wiring of the USB circuit was connected incorrectly.
Corrected the GND wiring and it worked normally.

0 Kudos
Reply