USB device, TRNG, AES

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB device, TRNG, AES

2,075 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MrBool on Tue Mar 29 07:12:38 MST 2016
I'm looking for LPC microcontroller with Cortex-M core, USB device, true random number generator and AES hardware support (SHA is also welcome). I can not find anyone. Does NXP not have such microcontroller?
标签 (1)
0 项奖励
回复
5 回复数

2,061 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复

2,061 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MrBool on Thu Mar 31 00:36:00 MST 2016
Thank you vtw.433e. You have right. I have made mistake during checking datasheet.
0 项奖励
回复

2,061 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Wed Mar 30 01:07:04 MST 2016
Eh? From the datasheet:
The LPC43S6x are ARM Cortex-M4 based microcontrollers for embedded applications which include an ARM Cortex-M0 coprocessor and an ARM Cortex-M0 subsystem for managing peripherals, up to 1 MB of flash and 154 kB of on-chip SRAM, 16 kB of EEPROM memory...

There is also the LPC18Sxx which has just a single Cortex-M3 and the same flash and peripheral options.
0 项奖励
回复

2,061 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MrBool on Wed Mar 30 00:57:27 MST 2016
Thanks for reply.  This family has big disadvantage for me - no flash.
0 项奖励
回复

2,061 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Tue Mar 29 09:25:20 MST 2016
LPC43Sxx is the family you are looking for.
0 项奖励
回复