USB dedicated LED outputs (LPC18xx/LPC43xx)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB dedicated LED outputs (LPC18xx/LPC43xx)

2,133件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wlamers on Mon Apr 15 05:56:22 MST 2013

THe LPC18xx/LPC43xx uC's have dedicated USB LED outputs (called USB0 port indicator LED control output, etc).


 


I have set the correct function number of the pins but there is no activity at all. I can, off course, set the LED's manually using the GPIO mode when the USB device connects/disconnects etc. But what is the point of having a dedicated mode for this? The manual is not mentioning anything at all about these outputs other then in the pin desccription in the USB section.


 


Anybody a clue what we can do with these LED outputs? And how to use them?

ラベル(1)
  • USB

0 件の賞賛
返信
2 返答(返信)

2,070件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wlamers on Tue Apr 01 00:21:10 MST 2014
Have had designed a PCB with them on. Seem to do nothing.
0 件の賞賛
返信

2,070件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Tue Apr 01 00:08:07 MST 2014
Same question.

What can I do with the Port Indicator LEDs? Is there an advantage to GPIO-controlled LEDs?

Regards,

Martin
0 件の賞賛
返信