USB data acquisiton / data streaming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB data acquisiton / data streaming

1,205件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by johnsmith on Tue May 01 06:49:13 MST 2012
I am trying to develop a High speed USB data acquisition device.  I am using the Hitex  LPC1850/4350 evaluation board populated with the LPC4350 chip.  I require an example of a data streaming application as a starting point.  My intention is to stream the collected data from the LPC4350 (device) to the PC (host) through Isochronous endpoints. If anyone could point me in the right direction, that  would be very helpful.
ラベル(1)
0 件の賞賛
返信
1 返信

1,184件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sjalloq on Thu May 03 08:41:05 MST 2012
The nxpUSBlib has an audio streaming OUT example but the library supports IN endpoints too.  The original Atmel based LUFA source had AudioIn examples.
0 件の賞賛
返信