USB communication with Libusb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB communication with Libusb

1,489 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rodri on Thu Apr 14 09:41:40 MST 2016
Hi,

I'm trying to communicate a link2 board with my PC. Up to this moment I have a CDC Vcom example based working, but the info transfers are at very low speed. I saw that Libusb can allow speeds up to 30 or 20 MBps, so my intention is to use that.

Can it works as a virtual Com port? if it don't, anybody can help me to understand how it works? It is my first time using USB, so I'm lost.
For the MCU part I'm using the LPCOpen example, but at the PC side I don't have any example. I'm using C# to program the interface application.

Thanks in advance!
regards,
Labels (1)
0 Kudos
Reply
1 Reply

1,281 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply