USB communication with Libusb

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB communication with Libusb

1,472 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rodri on Thu Apr 14 09:41:40 MST 2016
Hi,

I'm trying to communicate a link2 board with my PC. Up to this moment I have a CDC Vcom example based working, but the info transfers are at very low speed. I saw that Libusb can allow speeds up to 30 or 20 MBps, so my intention is to use that.

Can it works as a virtual Com port? if it don't, anybody can help me to understand how it works? It is my first time using USB, so I'm lost.
For the MCU part I'm using the LPCOpen example, but at the PC side I don't have any example. I'm using C# to program the interface application.

Thanks in advance!
regards,
标签 (1)
0 项奖励
回复
1 回复

1,264 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复