USB boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB boot

1,506件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sh on Sat Dec 10 05:30:30 MST 2011
According to the data sheet, the LPC43x0 supports booting via USB. No details are given, however. How does this work, what is the protocol used, and how can I try it using the Hitex eval board? I have tried to find information on the NXP site about this, but had no luck.

Cheers
Stefan
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,490件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpc18_43 on Wed Apr 04 13:45:46 MST 2012
USB DFU Download and Upload using DFU-Util works fine on the LPC18xx and LPC43xx:

http://knowledgebase.nxp.com/showthread.php?p=15454#post15454
0 件の賞賛
返信

1,490件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by trioflex on Mon Jan 23 04:44:45 MST 2012
Well UM says, DFU

But there seems to be DFU tool for LPC43xx ? So it seems we are stuck anyway...:(

Well the UART ISP boot works!

Need read the UM, and change SV1 setting to select USART0

send ?
get Syncrhonized
send Syncrhonized
get OK

send commands..


Antti
0 件の賞賛
返信