USB Virtual Com port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Virtual Com port

3,608 Views
kensu
Contributor V

Hi,

I have a problem with Virtual com port use.

I build the LPC1857 Virtual com port sample project, it work successfully.

But there is a problem with a procedure.

Step1: Power on 1857, and connect to PC with USB. PC will find a new com port.

Step2: Open Terminal Tool (I use TeraTerm), connect to this com port and start to receive/send data.

Step3: Re-connect USB line(also power RESET 1857), the terminal tool will not receive any data.

Step4: The terminal tool is still connected to this port, I close the terminal program.

Step5: Open terminal tool again, but it cannot find this com port. 

In Step5, I check the device manager, the com port is still exist. 

I think Step1 to Step4 is correct beahvior for common USB to Com device.

But Step5 is strange, I think the terminal should find the com port again.

Does it cause by firmware or driver? I think it's not terminal tool issue, because I check many common USB-UART port converter, they don't have this issue.

Thanks

Ken

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,904 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ken Su,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

I was wondering if you can tell me the information about your computer.

Did you ever try other terminal tools and can you replicate the issue on your colleagues' PC? And what's the results?

I'm looking forward to your reply.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,904 Views
kensu
Contributor V

Hello

Thanks for fast response.

My notebook is Windows 7 professional version (64bit) i5 CPU, Service Pack 1.

After check...

It can replicate for other PC or NB (all windows 7 system 32 or 64 bit).

I also check putty program, and another terminal tool made by C#.

Yes, the situation is same (100%).

Have any comment?

Thanks a lot.

Ken

0 Kudos
Reply

2,904 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ken,

Thanks for your reply.

I'd highly recommend you can refer to the USB CDC demo which is from the LPC18xx CMSIS-Compliant Standard Peripheral Firmware Driver Library and you may acquire some tips from it.

LPC18xx CMSIS-Compliant Standard Peripheral Firmware Driver Library (Keil, IAR) | www.LPCware.com
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply