USB V-Com driver problem with Windows - 8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB V-Com driver problem with Windows - 8

2,139 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Mon Nov 16 23:48:50 MST 2015
Hi,
I have project using USB V-Com, in which I' am using LPC4088 microcontroller. I used library and driver provided from LPCExpresso(RDB4078_NXPPDL_Examples), it was working fine with Windows 7, but when I tried to install the driver on Windows 8, I' am getting and error message as "The third party INF file doesn't contain digitally signed information". Where can I get digitally signed driver for USB V-Com? Or How can I solve this problem?
Labels (1)
0 Kudos
Reply
3 Replies

2,106 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Wed Nov 18 07:37:13 MST 2015
Have you modified them in any way? Such as using a different vid/pid? If so, it is up to you to re-sign them. Any modification, no matter how trivial, to the inf file will require it to be re-signed.

I can confirm the standard link2 drivers work on Windows 8 and Windows 10.
0 Kudos
Reply

2,106 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sixten11 on Wed Nov 18 06:03:59 MST 2015
I use the Link 2 drivers on Windows 7 (with LPC43xx), they should work on Windows 8 too.
0 Kudos
Reply

2,106 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Tue Nov 17 03:01:06 MST 2015
Driver signing in Windows 8 and later can be a right PITA.

You might want to take a look at the LPCOpen package for LPC40xx :

[list]
  [*]https://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc40xx-packages
[/list]
along with the drivers at:
[list]
  [*]https://www.lpcware.com/content/nxpfile/lpcxpresso-link2-usb-driver-package
[/list]

HTH!
0 Kudos
Reply