USB Transmit and recive buffer size (LPC1822)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Transmit and recive buffer size (LPC1822)

1,553 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Brady on Thu Aug 29 02:13:29 MST 2013
Hello,

I will use the HS USB periperal. (USB0)

I have a question.

How much is the transfer buffer size at one time? (USB DEVICE MODE)

You can be found the buffer size(128words) in the User's Manual.

Please refer to the attached file.

I want to transfer 512byte at one time.

Please, inform to me.

Thanks & Regards.
Labels (1)
0 Kudos
Reply
1 Reply

1,530 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Thu Aug 29 02:59:10 MST 2013
Unless my math is wrong, 128 words IS 512 bytes
0 Kudos
Reply