USB TO SD CARD? POSSIBLE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB TO SD CARD? POSSIBLE?

1,272 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vahid_22002 on Tue Aug 18 13:35:51 MST 2015
hello dears,
I have a project in which I should copy a file from sd card and then write into usb flash device.
I use lpc1768.
Is it possible?
I should note that I use rl arm library.
thank you for our replies.
Labels (1)
0 Kudos
Reply
1 Reply

1,228 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Wed Aug 19 05:43:33 MST 2015
[list]
  [*]  LPC1768 can be USB host --> you can connect a USB stick if you have the right software for it (mass storage). Keil RL should make it.
  [*]  There is no SD card interface in the LPC1768 --> you can use SPI to talk to the card
[/list]

If there is something like that already available? I don't know. Maybe you should perform an internet search for it.

Regards,
NXP Support Team
0 Kudos
Reply