USB ROM Driver - Detect Attach and Removal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB ROM Driver - Detect Attach and Removal

833 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by emh203 on Wed Nov 19 12:28:36 MST 2014
Is there a clean way to determine when a USB device is attached or removed with the USB rom drivers?   I am currently using MSC.    I need to be able detect when the enumeration process is complete and when the device is disconnected to be able to provide some mutual exclusion when accessing the SD card.

The dirty way to do it is monitor VBUS on an IO pin but I was hoping to there was a way through the ROM drivers.    I am pretty sure I can get what I want by adding code to a custom interrupt handler but I wanted to see if there were callbacks available for this function.

标签 (1)
0 项奖励
回复
0 回复数