USB OTG on LPC54606 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB OTG on LPC54606 ?

1,678件の閲覧回数
gph
Contributor III

Hi,

Is it possible to use USB On The Go on LP54606 ?

I don't find any schematic and not really response in user manual.

Thanks a lot.

Philippe.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,584件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Philippe GRAILLE,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Q1) Is it possible to use USB On The Go on LP54606 ?
-- No, so I'd recommend you to consider using the LPC43xx series to replace the LP54606.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信